AddResourceRequirementProperties (IProductionRuntime)
Adds named properties of the resource as resource requirement properties.
Inputs | Data Type | Description |
---|---|---|
Property Names | String[] |
Specifies the names of the properties' input parameters to add. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Requirement Id | GUID |
Specifies the value for the resource requirement to add the properties to. This is the ID that is returned when you create a segment response. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Resource Type | Dependent on each parameter's data type | Specifies the resource type of the resource actual being written to. There are three options:
|