AddResourceActualProperties (IProductionRuntime)

Adds named properties of the resource as resource actual properties.

InputsData TypeDescription
Actual IDGUID

Specifies the value for the resource actual to add the properties to. This is the ID that is returned when you create a segment response.

In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use.

Property NamesString[]

Specifies the names of the properties' input parameters to add.

In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use.

Resource TypeDependent on each parameter's data typeSpecifies the resource type of the resource actual being written to. There are three options:
  • Material
  • Equipment
  • Personnel