CreatePersonnelActual (IProductionRuntime)

Creates a personnel actual on a specified segment response, without the ability to set initial start and end time values for the actual.

If you want to set initial start and end time values for the actual, use the CreatePersonnelActualEx call method instead.

Note:
The S95 ID must be unique in the system or the call method fails.
InputsData TypeDescription
DescriptionDirectoryResource

Specifies the description of the personnel actual.

PersonnelString

Specifies the name of the person or personnel class associated with the personnel actual.

In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use.

QuantityDouble

Specifies the quantity of the personnel resource actual used.

Requirement IDGUID

Specifies the resource requirement you want to associate with the personnel actual.

S95 IDString

Specifies the unique name of the personnel actual on the specified segment response.

Segment Response IDGUID

Specifies the segment response you want to associate with the personnel actual.

Unit of MeasureString

Specifies the unit of measure for the quantity you want to associate with the personnel actual.

OutputsDescription
GUID 

Returns the new personnel actual.