CreateWorkResponse (IProductionRuntime)
Creates a work response based on a specified work definition.
Note:
Multiple process segment responses can be associated with a work response.
Inputs | Data Type | Description |
---|---|---|
Description | String | Specifies the description of the work response. |
Location | DirectoryResource |
Specifies the equipment location to associate with the work response. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
S95 ID | String | Specifies the name of the work response. |
Work Request | DirectoryResource |
Specifies the work request to associate with the work response. This can be empty if there are no work requests to associate with this response. |
Work Type | String | Specifies the work type of the work request you are associating with the work response. Valid values are:
On the Configure Method dialog box, click Next to select a work type. You cannot select or enter a work type on the activity configuration panel. |
Outputs | Description | |
---|---|---|
GUID | Returns the new work response. |