AddWorkDataClassToResponse (IProductionRuntime)
Adds work data from a work data class to a segment response.
Note:
If you add a work data class that the process segment does not have, when you try to write a value to it, the write fails and no values are recorded. The data class must be an optional data class in the process segment definition.
Inputs | Data Type | Description |
---|---|---|
Segment Response ID | String |
Specifies the segment response you want to add a work data class to. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Work Data Class | String |
Specifies the work data class to add to the segment response. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |