WriteResourceRequirementProperties (IProductionRuntime)
Writes properties to a specific resource requirement.
Note:
In the Configure Method dialog box, click Next to select a resource actual and its properties you want to write. You can select all properties or a subset. Each property you select displays as an input parameter on the activity configuration panel.
Inputs | Data Type | Description |
---|---|---|
Requirement ID | GUID |
Specifies the value for the resource requirement to add the properties to. This is the ID that is returned when you create a segment response. In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use. |
Resource Type | Dependent on each parameter's data type | Specifies the resource type of the resource requirement being written to. There are three options:
|