ReadSegmentRequirements (IProductionRuntime)

Reads the attributes of segment requirements for a specific work request.

InputsData TypeDescription
Detail LevelSegmentRequirementsDetailsLevel
Specifies the detail level of the output. Valid values are:
  • SegmentsOnly
  • IncludeParameters
  • IncludeEquipmentRequirements
  • IncludeMaterialRequirements
  • IncludePersonnelRequirements
  • ChildrenOnly
  • FullDetails
Work RequestDirectoryResource

Specifies the work request with the segment requirement attributes you want to read.

In the Inputs section of the activity configuration panel, click the ellipsis button to open the Universal Browser to select the resource you want to use.

OutputsDescription
SegmentRequirementCollection 

Returns the segment requirement attributes.

Use a For Each Activity to loop through all resources or use an Index Activity to find a named segment.

Note:
Work parameters are the properties that can be indexed.
Important:
The returned collection of data is based on user-defined values and is dependent on your published data. Each segment requirement can contain work parameters, as well as material, equipment, and personnel requirements. For information on the attributes that can be read from, see Work Requests.