Installing the License Client

You can install the License Client using the command line.

Procedure

  1. Open a command-line interpreter window with Administrator privileges.
  2. Enter the following:
    start /wait ProficyClientInstaller.exe /nomsg /quiet
    
    If you do not want Sentinel USB drivers installed, add /nousbdrivers to the above command line. These drivers are required if you are using a M4, M5, or configurable (Advantage) USB hardware key.