Activating Licenses from the Cloud Server
Before you begin
About this task
Note:
You may activate one or more activation codes by separating them with a
semicolon. Do not use spaces between the activation codes.
Procedure
-
To activate licenses from the command line:
You should receive the following response:
"License(s) were deployed successfully."Note:If there is an error executing the command, a message appears. For more details, see the Proficy License Client log file. -
To activate licenses using a batch file, enter your commands in the following format in
your batch file:
echo off Start/wait ProficyLicenseWizard.exe -ActivateFromCloud=1111-1111-1111-1111;2222-2222-2222-2222 if errorlevel 1 ( echo The command failed. Error code=%errorlevel% exit /b %errorlevel% ) echo Success