USB Key Overview
- Non-configurable USB hardware key
- Configurable USB hardware key (legacy)
Non-configurable USB hardware key
Non-configurable USB hardware keys or M5 Keys are pre-loaded with the licensing information for your products. You cannot modify the licensing information contained in these keys. However, if you need additional licenses, you can purchase them from GE Vernova and then re-flash keys with a GE Vernova-supplied image file that overwrites all existing information and replaces it with updated licensing information.
Configurable USB hardware key
Configurable USB hardware keys will continue to be supported by GE Vernova. These configurable keys are plugged into computers connected to the Internet in order to activate licenses on them. Once activated, a USB key can be used to license a physical or virtual computer that does not need to online. However, changes, upgrades, or returns require the key to be plugged into a computer connected to the Internet so the Licensing Server can be accessed. The final legacy licensing option, Keyless software licenses, continues to be supported by GE Vernova but will eventually be phased out.