Operation and Task Status Messages
These tables describe the status messages you see when performing operations in Edge Manager.
The following table describes the status messages you see when operations are performed.
Message | Description |
---|---|
Pending | All tasks have a pending status before an operation starts. |
In Progress | When one or more tasks begins progress, and some tasks are successful, some are pending, and no failure occurs, a number displays how many are still incomplete, for example: In Progress (4) . |
Successful | When all tasks under an operation are successful. |
Failed | When any one task in an operation fails, a number displays how many tasks have failed, for example: Failed (2) . |
Unknown | All of the tasks in an operation are unknown. |
The following table describes the status messages you see when tasks are performed.
Message | Description |
---|---|
Pending | The task has not started. |
In Progress | The task is in progress. |
Timeout | The task timed out prior to completion. |
Success | The task completed successfully. |
Cancelled | The task was cancelled. |
Failed | The task failed to complete. |
Unknown | A task can "lose" its status if the back-end service goes down while something is in progress. The task may or may not recover its status. For example, if the task was in progress, it may eventually finish, which will fix it. This status is rare. |