Modify a specification in work definition segments

Procedure

  1. In the navigator, click Production.
  2. In the Folders list, select the resource type you want to work with.
    Tip:
    As more lists appear, select the appropriate resource until you find the one you want to work with.
  3. In the Displays panel, click S95 Model Editor.
  4. Click the Specifications tab, and then select a specification.
  5. If applicable, click Select to select a new resource.
    • Using the Universal Browser, select a resource, and then click OK.
    • Click Clear to remove the selection.
  6. In the Quantity field, enter a new amount.
  7. Click Save.