Work Definition Segment Parameters Tab

The Parameters tab allows you to add, modify, and delete parameters that are specific to the selected work definition segment, and to view the parameters for the associated work process segment.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
List User-defined

Displays a list of parameters for the selected resource that can be arranged by name, type, and so on, depending on the parameter. These parameters can be inherited from another resource or created for the current resource.

Add ParameterN/A Click to add a new parameter.
Delete Selection N/A Click to remove the selected parameter.
Name User-defined alphanumeric string (A–Z, a–z, 0–9) up to 50 characters Specifies a display name for the selected parameter.
Description User-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 characters Provides more information about a parameter that a user may find helpful.
Data Type System-defined Specifies the data type of the parameter.
Note:
This parameter cannot be changed if it is inherited from another resource.
Value User-defined alphanumeric string (A–Z, a–z, 0–9) up to 255 characters Specifies the value for the selected data type. Valid values depend on the selected data type.
Unit of Measure User-defined alphanumeric string (A–Z, a–z, 0–9) up to 20 characters Specifies the unit of measure for the data type, such as gallons, inches, tons.