Work Definition Segement Specifications Tab

The Specifications tab for the selected work definition segment displays the equipment, material, and personnel specifications inherited from the associated work process segment.

When process segment specifications are modified, added, or removed, this information is reflected in the specifications tab of the associated work definition segments. However, you can modify select information related to the specification, such as the quantity and a non-class resource.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Specifications listUser-defined Displays a list of associated equipment, material, and personnel resources that can be sorted by name or type.
Select Equipment buttonN/A Click to open the Universal Browser to define this resource more specifically by selecting a non-class resource.
Select Material buttonN/A Click to open the Universal Browser to define this resource more specifically by selecting a non-class resource.
Select Personnel buttonN/A Click to open the Universal Browser to define this resource more specifically by selecting a non-class resource.
Settings: Quantity fieldUser-defined numeric value Specifies the required quantity for the resource.
Clear buttonUser-defined Click to remove the newly selected resource.