Work Definition Segment Details Tab
The Details tab offers general information about the selected work definition segment.
You can change the name and description of this resource.
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
The following table describes the attributes specific to this resource type.
Attribute | Value | Description |
---|---|---|
Related Work Process Segment | User-defined | Specifies the process segment associated with the definition segment. |
Work Definition Segment Duration: Duration | User-defined numeric value | Specifies the resource's duration in minutes. The duration can be defined at any level of the process. Duration is not inherited through an association with another resource. |
Set as Master Segment | User-defined | Specifies whether the work definition segment is a master segment. This check box is read-only. You can set the master segment on the Work Process Segments Details tab. |