Create a segment hierarchy
Before you begin
Important:
A work definition segment cannot be a child of another work definition segment if it is already a parent to that segment. As well, a work definition segment cannot be a parent to another work definition segment if it is already a child of that segment.
Procedure
- In the Navigator, click .
- From the Work Definition Segments list, select the resource you want to work with.
- In the Displays panel, click S95 Model Editor.
- On the Child Segments tab, click Associate child segment.The Universal Browser appears.
- From the resource list, select the work definition segment you want to associate with the current work definition segment, and then click OK.Tip:To remove a segment association, select the appropriate child work definition segment, and then click Remove child segment.
- If applicable, click Edit, and then in the Name field, enter a name for the segment association.
- In the Order field, enter the execution order for the associated child work definition segment.
- Click Save.