Filtering Devices by Group

In Edge Manager, you can filter the device list in Device Manager to view and perform actions on only devices in a specified group.

About this task

By default, the Device Manager > Devices page displays all devices.

Procedure

  1. In the left navigation pane, select Device Manager > Devices.
  2. Click the filter icon .
  3. In Filter Scope, select the group to view devices for.
    If the group you selected has subgroups (children), The Select All Sub-Groups drop-down list appears. You can check the box on the left to select all sub-groups, as shown in the below image.
    You can also expand the list of sub-groups, and select only specific sub-groups, as shown in the below image.
    Note:
    If the group you selected has subgroups, devices belonging to the subgroups are not added unless you select this option. If you select this option, when you deploy the BOM, it is deployed to all the subgroups and all the devices in the subgroup.
  4. Click Apply.
    The device list is updated so that only devices in the selected groups appear in the device list.
  5. (Optional) Click Save to save the filter for future use.
    1. Enter a name for the filter.
    2. (Optional) From Device Filters select attributes from the list to further narrow filter results.
    3. Click Save.
      Your filter appears in the Saved Filter Sets list.