Deploying a Bill of Materials to a Single Device
Use the Device Manager page to deploy a BOM to a single device.
Procedure
- In the left navigation pane, select
.
- Click the link for the device to which to deploy the BOM.
- Click the BOM tab.
- Select Deploy BOM.
- In the Select BOM dialog box, select the BOM to deploy, and click Schedule.
If there are multiple versions of the BOM file, you can click in the version column to select the version of the BOM to deploy.
When a BOM is updated and redeployed, packages specified in the BOM that are already installed on the device are skipped (not downloaded and deployed again). Only new packages are deployed to the device. The status of skipped packages is displayed as "installed" rather than "success."
Note:If you schedule a deployment to a device with the status of "created" or "offline," the status displays "Pending" until the device comes online, at which time the deployment begins automatically and the status changes to "In progress." - In the Schedule Software Deployment dialog, select the date and time for deployment to the device.Note:You can set the time zone timestamp formatting (UTC or local) in the Settings page.The Deployment Status dialog appears.
- In the Deployment Status dialog box, click Close.The BOM deployment appears in the Last Created Operation section.