Deploying Edge Apps
In Edge Manager, you can deploy edge apps to multiple devices at once, or to single devices.
Procedure
- In the left navigation pane, select
.
- To deploy edge apps to a single device, follow these steps.
- To deploy edge apps to multiple devices, create and apply filters to the device list, or select multiple devices, then select
- In the Select Edge Applications dialog, select the applications to deploy and click Next.
- In the Add Edge Applications Identifiers, add the unique application identifiers for the app, then click Next.If you are deploying multiple instances of the same edge app on a single device, each edge app instance must have a unique Application ID. When you deploy configurations, you must know the App ID for the instance of the edge app to which to apply the configuration.Application IDs must follow these rules:
- Must begin with an alpha-numeric character.
- Must be 50 characters or less.
- Can consist of alpha-numeric characters, hyphens and underscores.
The Schedule Deployment dialog box appears. - In the Schedule Deployment dialog, select the date and time for deployment to the device.Note:You can set the time zone timestamp formatting (UTC or local) in the Settings page.