Set a task step to be automatically acquired

Procedure

  1. In the navigator, click Workflow.
  2. In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
  3. In the resource type list, select a resource.
  4. In the Displays panel, click Workflow Management > Workflow Editor.
  5. Click the Workflow Editor tab.
  6. Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.
    Note:
    If required, configure the workflow.
  7. From the subprocess configuration panel. click the General tab.
  8. Select the Automatically acquire task step check box.
  9. To remove this setting, clear the Automatically acquire task step check box.
  10. Click Save.