Subprocess Configuration Panel-Within the Subprocess
When you are inside a subprocess, you can configure attributes that are specific to the subprocess. You can access the internal subprocess from the Workflows folder, or from the Subprocesses folder, in the Workflow model.
Tip:
You can use a Write Activity to change some property values at run
time.
Inputs and Outputs
As the subprocess author, you define the attributes and values of the input and output parameters. There are no system-defined attributes.
Panel Attributes
The following table describes the available options.
Attribute | Value | Description |
---|---|---|
View | User-defined | Allows you to choose between two views:
|
Default Completion Code | User-defined | Click the ellipsis to add a preconfigured completion code. |
User-defined | Click the Edit link to configure. | |
User-defined | Click the Edit link to configure. | |
User-defined | Click the Edit link to configure. | |
User-defined | Click the Edit link to configure. | |
User-defined | Click the Edit link to configure. | |
User-defined | Click the Edit link to configure. |