Add a registry patch
About this task
The Mobile-sized Task List supports opening files inside browser windows. However, with Microsoft Office 2007 and later, some applications (such a Word, Excel, and PowerPoint) open only outside the browser window regardless of settings. Therefore, opening these file types using the Mobile-sized Task List does not work.
To open these files inside a browser window using the Mobile-sized Task List, apply the following registry patch. These registry settings must also be on the machine that the mobile client is deployed to.
Procedure
- Open a text editor.
- Copy and then paste the following text into the editor:
Windows Registry Editor Version 5.00 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Word.Document.8] "BrowserFlags"=dword:80000024 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Word.RTF.8] "BrowserFlags"=dword:80000024 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Word.Document.12] "BrowserFlags"=dword:80000024 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Word.DocumentMacroEnabled.12] "BrowserFlags"=dword:80000024 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Excel.Sheet.8] "BrowserFlags"=dword:80000A00 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Excel.Sheet.12] "BrowserFlags"=dword:80000A00 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Excel.SheetMacroEnabled.12] "BrowserFlags"=dword:80000A00 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\Excel.SheetBinaryMacroEnabled.12] "BrowserFlags"=dword:80000A00 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.Show.8] "BrowserFlags"=dword:800000A0 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.Show.12] "BrowserFlags"=dword:800000A0 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.ShowMacroEnabled.12] "BrowserFlags"=dword:800000A0 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.SlideShow.8] "BrowserFlags"=dword:800000A0 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.SlideShow.12] "BrowserFlags"=dword:800000A0 [HKEY_LOCAL_MACHINE\SOFTWARE\Classes\PowerPoint.SlideShowMacroEnabled.12] "BrowserFlags"=dword:800000A0 [HKEY_CURRENT_USER\Software\Microsoft\Windows\Shell\AttachmentExecute\{0002DF01-0000-0000-C000-000000000046}] "Word.Document.12"=hex: "Word.Document.8"=hex: "Excel.Sheet.8"=hex: "Excel.Sheet.12"=hex: "PowerPoint.Show.8"=hex: "PowerPoint.Show.12"=hex:
- Save the file as FileName.reg.
- Double-click FileName.reg to run this registry script.
- Restart the Mobile-sized Task List.
- Start Microsoft Internet Explorer.