Set a subprocess task step to expire
You can set an expiration date and/or time for subprocess task steps when a workflow is running.
Procedure
- In the navigator, click Workflow.
- In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
- In the resource type list, select a resource.
- In the Displays panel, click .
- Click the Workflow Editor tab.
- Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.Note:If required, configure the workflow.
- From the subprocess configuration panel, click the Task Step Details tab.
- From the Expiration Type drop-down list, select:
- Relative to set a countdown
- Absolute to set an exact expiry time
- For a relative expiration:
- In the Duration field, set the number of days, hours, minutes, or seconds until the expiration.
- To set a conditional event, select the Condition Event check box.
- Click Configure Event.
- For an absolute expiration:
- In the Duration field, enter a date and time.
- Click OK.
- If required, create an expression or perform a bind to set parameter values.
- Click Save.