Schedules

Schedules are used to run a workflow when an event occurs and provide more configuration options for specific workflows. However, they are created and executed separately from workflows.

Schedules can be used to override values configured for a workflow, such as task priority, work instructions, assignments, expiration, and linked documents. They also provide the ability to enter literal values for workflow input parameters, as well as bind to variables and event properties.

There are four configuration tabs in Workflow Schedules: details, parameters, task details, and tracking configuration. Each tab, starting with Details, works in succession and inherits the original properties of the task details for the selected workflow.

Example

You have a workflow called Machine Cleaning. This workflow is used to clean a number of different models of mixers. A supervisor selects the workflow, assigns a role, location, and input parameters, and then schedules it for a particular day. The workflow is given context with a role, location, the mixer model to clean, and point in time to execute. When the workflow event and schedule are enabled, the schedule is available to be executed.

Note:
You can configure up to 3000 schedules.