Schedule Parameters

The parameters available in Workflow Schedules are the preconfigured input parameters or data items of the selected workflow. If the selected workflow has no parameters, no information displays on this tab.

Note:
Subprocess level parameters and fault handler parameters are not displayed in the workflow schedule parameters list.

Schedule parameters can be set with a static initial value for the parameter, or can be bound to any variable or event property (if an event is attached to the schedule). The values and the types of values available to be configured depend on the selected workflow. A parameter reconfigured in Workflow Schedules is saved as part of the schedule configuration and overrides the workflow parameters.

Schedule Parameter Overrides

Note:
If any parameter types are changed in an attached workflow after that workflow was attached to the schedule, the original workflow parameters displayed in the schedule appear as invalid.

The following table shows the options available when modifying the input parameters:

AttributeValueDescription
Parameters for WorkflowUser-definedDisplays a list of available input parameters for the selected workflow.
ParameterUser-definedSpecifies a value for the selected parameter. Field options vary depending on the parameter's data type.
Data SourcesUser-definedFrom the drop-down list, select Data Source to open the Configure Data Source window, and then select a resource to bind to.
Event SourcesUser-definedFrom the drop-down list, select Event Property to open the Event Properties dialog box, and then select a resource to bind to.
Note:
This option is available only if an event is attached to the current schedule.
Tip:
The system prevents you from entering an invalid value or selecting an invalid binding.