User Interface Attributes for Schedules

The Overview tab provides general information about the currently selected schedule.

You can select a workflow to be scheduled, as well as the options related to how the schedule starts. Schedules are executed based on a timed event, conditional event, production event, or a manual trigger.

When you create a schedule, you must completely configure all elements, except Version, on the Overview tab. Here, you select the workflow to be scheduled, and then you can either assign an event to trigger the schedule, or you can manually run the schedule.

Note:
Only elements on the Overview tab require configuration. The other tabs in schedules are optional.

Schedule Configuration

The following table describes the available options.

AreaValueDescription
Select Workflow: BrowseUser-definedClick to open the Universal Browser to select the workflow you want to schedule.
Note:
If you select a disabled workflow, this schedule cannot run.
Schedule by Event: BrowseUser-definedClick to open the Select Event dialog box to select an event to trigger the workflow schedule. This button is available only when a workflow is selected.
Tip:
For information on configuring scheduled events from Workflow Schedules, see Event Sources.
Schedule by Event: DeleteN/AClick to remove the selected event. This button is available only when an event is selected.
Manual Trigger: Run WorkflowN/AClick to manually start the selected workflow. This button is available only after a workflow is selected and the schedule is enabled.
Start Task FilterN/ASpecifies the location and/or personnel to filter the list of tasks presented when you click the Start Task button.