Assignments in Schedules
The Assignments area is where you can override the previously configured location/personnel assignments for workflow tasks or subprocess task steps, depending on the requirements of the schedule. These task/tasks steps can be sent to an assigned computer or operator at that station to complete.
Note:
The schedule must contain either a personnel or location assignment, but it can also contain both. When you clear an assignment, the original workflow assignment is not retained.
Attribute | Value | Description |
---|---|---|
Original Task/Task Step Assignments | System-defined | Displays the original equipment and personnel assignment configurations for the selected task or task step. |
Override | N/A | Select this check box to update the schedule. |
Set Location | User-defined | Click to select an equipment or computer resource for the selected workflow task or subprocess task step. |
Set Personnel | User-defined | Click to select a personnel or personnel class resource for the selected workflow task or subprocess task step. |
Clear | N/A | Click to remove location or personnel settings. |