Override work instructions for a schedule

Procedure

  1. In the navigator, click Workflow > Schedules.
  2. In the resource type list, select a resource.
  3. In the Displays panel, click Workflow Management > Workflow Editor.
  4. Click the Task Details tab, and then click the Work Instructions tab.
  5. In the Task/Task Steps panel, select:
    • The workflow to add different instructions to the task.
    • A subprocess to add different instructions to the task step.
  6. Select the Override check box.
  7. In the new workspace, enter work instructions.
    Tip:
    You can insert information copied from another application, as well as graphics, but it cannot exceed 4 MB.
  8. Click Save.