Modify your application server database
The Configure Database tool provides the ability to make changes to your SQL Server database, as well as change the database you want to connect to.
Before you begin
You must install SQL Server before you install Workflow. For more information, see Software Requirements in the Workflow IPI documentation.
About this task
In order for Workflow to connect to Microsoft® SQL Server at runtime, you must configure SQL Server to enable the db_owner role for the applicable login account. For more information, see Enable Connection between Workflow and SQL Server.
The Workflow installation automatically selects the default SQL Server instance. For example, if SQL Server 2012 and SQL Server 2008 are both installed, SQL Server 2008 may be the default instance. In this scenario, if you want to use SQL Server 2012 instead, you must select this instance as the default as part of manually configuring your SQL Server settings. For instructions, see steps 2 and 3 of this procedure.
Procedure
- Click Start > All Programs > General Electric > Workflow > Configuration > Configure Database.The Database Configuration page appears.
- Specify the SQL Server database settings for this application based on the configuration of your environment.
To configure SQL Server settings... Then... Automatically - Select the Use a local database with Windows Authentication check box.Note:To use this option, the following SQL Server conditions apply:
- Installed locally, AND
- Designated as default Local Host, AND
- Uses Windows Authentication
- Proceed to step 4.
Manually - Clear the Use a local database with Windows Authentication check box.
- Proceed to step 3.
- Select the Use a local database with Windows Authentication check box.
- Specify your SQL Server settings, as follows:
- Click Save, and then click Exit.