Modify the Microsoft Active Directory Services
The Configure AD LDS Integration tool provides the ability to configure Active Directory Lightweight Directory Service for your production environment.
Procedure
- On the server machine, click .The AD LDS Integration page appears.
- To integrate Active Directory Lightweight Directory Services (AD LDS), do one of the following.
If AD LDS is... Then... NOT installed You are given information regarding its use. If it is not required, then click Next. Installed in a test and/or development environment Select the Do not use Microsoft Directory Services check box, and then click Next. Installed in a production environment Click Next. - If you are using AD LDS, perform the following procedure:
- Clear the Do not use AD LDS check box.
- In the Directory Instance section, in the Name field, enter an instance name for the ADAM directory.
- In the Port (LDAP) and Port (SSL) fields, enter valid port numbers.
- In the User Credentials section, in the Name field, enter the name of a user that is a member of the local computer's Administrators Group.
- In the Domain field, enter the name of your company's domain.
- In the Password field, enter the password for the user you entered in the Name field.
- Click Save, and then click Exit.