Upgrading Workflow
Please refer to the WorkflowIPI PDF for information on upgrading Workflow, compatibility with earlier versions and other GE Products. Read this topic for general information about upgrading your applications.
Upgrade Paths
- From Workflow 2.5 SP4 to Workflow 2.6
- From Workflow 2.5 SP3 to Workflow 2.5 SP4
- From Workflow 2.2 SP2 to Workflow 2.5 SP4
- From Workflow 2.5 SP1 to Workflow 2.5 SP4
- From Workflow 2.5 to Workflow 2.5 SP4
- From Workflow 2.5 SP2 to Workflow 2.5 SP3
- From Workflow 2.5 SP1 to Workflow 2.5 SP3
- From Workflow 2.5 to Workflow 2.5 SP3
- From Workflow 2.2 SP1 to Workflow 2.5 SP3
- From Workflow 2.5 SP1 to Workflow 2.5 SP2
- From Workflow 2.5 to Workflow 2.5 SP2
- From Workflow 2.5 to Workflow 2.5 SP1
- From Workflow 2.1 to Workflow 2.5
- From Workflow 2.2 service pack 1 (SP1) to Workflow 2.5
- From Vision 6.2 to Vision 6.3Note:All versions of Vision prior to version 6.3 must be uninstalled before being upgraded to Workflow 2.5 SP1.
- From Workflow 2.1 to Workflow 2.2 service pack 1 (SP1)
- From Workflow 2.0 to Workflow 2.2 service pack 1 (SP1)
- From Workflow 1.5 service pack 4 (SP4) to Workflow 2.2 SP1Note:You must first upgrade Workflow 1.5 SP4 to Workflow 2.0.
If you are upgrading from an earlier version of Workflow, contact Technical Support.
GE Historian
If you use GE Historian as a data source, then when you upgrade Workflow to v2.5 SP2 the existing GE Historian server address is automatically displayed in the Server Name field in the Data Source Editor. You cannot change the server's alias (that is the name displayed in the Historian Servers list in the navigator). To change the alias, you must delete the connection, and then add a new one. For more information, see Change the Historian Server and Add an Historian Server.
Legacy Certificates
Starting with Workflow 2.5, legacy certificates are no longer supported.
Upgrading Extension Servers
If you are installing or upgrading an extension server (Workflow or User), you must have already installed or upgraded an application server of the same version to host the Core services on a separate machine
Upgrading Microsoft® .NET Framework 4.5 (Full Framework)
- For an assembly that pre-dates .NET 4.0, you must upgrade the assembly when you open it. Failure to do so results in an error and the inability to save the edited assembly.
- For an assembly that targets .NET 4.0, the assembly is upgraded automatically when opened, and changes to such assemblies can be saved as before.
Service providers that target versions of the .NET framework before version 4.5 must be recompiled targeting .NET 4.5.
Upgrading Web-based Forms for the Task List
Upgrading a Clustered Environment
After upgrading Workflow on the primary server machine, you must reconfigure that machine as the primary server (see Configure the Primary Cluster Server) in the cluster, as well as reconfigure the failover server (see Configure the Failover Cluster Server) in the cluster.
SQL Server Database Replication
When upgrading the application, if you are using a replicated database and have replication turned on, you must turn it off, upgrade, and then turn it on again. You must also upgrade the replicated database. For more information, see Upgrade a replicated database.
Password Security
During an upgrade installation, the account lockout capability is automatically enabled; all other password security features are disabled, by default. To enable any of the other password security features, you must use the Configure Security tool after the upgrade installation has successfully completed.
Windows Users
Workflow 2.0 supports Windows domain names with personnel names and login names. If you choose to use the new functionality included with Workflow 2.0 (that is, active directory universal or global groups mapped to Workflow groups), then when your Windows users log in, their personnel name and login name will both be updated to include the domain name, and the personnel name will change to match the login name. For example, the personnel name John Smith and login name johnsmith will both change to <domain name>\johnsmith.