Change architecture mode

When initially installing an application server or extension server (that is, Workflow or User) on a 64-bit computer, you can elect to run the server in either 32-bit or 64-bit mode. If your environment changes subsequent to installation, you can use the Configure Server tool to change the architecture mode accordingly.

Procedure

  1. On the machine that the server is installed on, click Start > All Programs > General Electric > Workflow > Configuration > Configure Server.
    The Configure Server tool appears.
  2. Select the Create an Application Server Instance option.
  3. Click the Advanced Configuration arrow.
  4. In the Run service under the following architecture section, select 32-bit or 64-bit to indicate the operational mode you want to switch to.
  5. Click Save, and click Exit.