Link external documents to task steps

For each step in a task, you can add external documents to be available from the Task List during run time. Linked documents are only available to users once a task step starts running.

About this task

Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.

Procedure

  1. In the Task Editor, click the Linked Documents tab.
  2. Select the listing for the task step that you want to specify related external documents for.
  3. Click Add Linked Doc.
    Note:
    You can only add the number of documents that the related workflow (associated template) allows. You can view the maximum number at the bottom of the list pane. If the Add Linked Doc button is inactive, the maximum number of documents has been reached.
  4. In the Display Name field, enter the name that you want to be displayed in the Task List to identify the linked document at run time.
    Note:

    For this and any other field containing text that may be displayed in the Task List, you can type Keywords as part of your entry. For more information, see Use keywords in eSOP task text.

  5. Near the URL/UNC field, click Browse, and then in the displayed dialog box, navigate to and select the document.
    Note:
    If you know the absolute path or full web site address for the document, you can enter it directly in the field instead.
  6. Optional: To view the document or web site, click Preview.
  7. Click Save.
  8. To add additional external documents, perform one of the following procedures.
    • For the currently selected task step, repeat steps 3 through 7.
    • For a task step other than the currently selected one, repeat steps 2 through 7.