Use keywords in eSOP task text
For any field containing text that may be displayed in the Task List, as well as for the subject and body of task-related email messages, you can type Keywords as part of your entry. At run time, keywords are replaced in the Task List with parameter values specific to the given task or task step, such as the name of the user who is performing the current activity.
Procedure
- In the Task Editor, click the task listing, and then click Keywords tab.A read-only grid appears, displaying a list of keywords configured for the workflow template that the task is associated with.
- For each keyword that you want to use, make note of the corresponding name.
- If you want to use the keywords in relation to a task step, select the listing for the step.
- Click the tab containing the text field where you want to include keywords as part of your entry, and then click in the field itself.
- In the text location where you want the parameter value for the keyword to appear, enter the keyword, using the convention <@Keyword@>.