Disable a task schedule

If a schedule is no longer applicable to a task, you can disable the schedule. If the schedule is the only one configured for the task, disabling the schedule deactivates the task. You can see schedule activation state under the schedule name on the Schedules tab.

Procedure

  1. In the Task Editor grid, click the listing for the task you want to modify.
    Tip:
    If the grid interface is not displayed, click the Task button. If you do not see the task listing in the grid, expand the group that the task belongs to by clicking the downward-pointing arrow beside the group listing.
  2. Click the Edit button.
    The editing interface appears in the Task Editor workspace.
  3. Click the Schedules tab.
  4. Select the listing for the schedule that you want to disable.
  5. In the Status area, click Disable.
  6. Click Save.
    The schedule is disabled.
    Note:
    If the schedule is the only one configured for the task, the task is deactivated.