Configure task emails
You can configure email messages to be sent upon initiation and/or expiration of an overall task or individual task steps, as required.
Before you begin
- Prerequisites
- Create and link a task
- Add task steps
About this task
Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.
Procedure
- In the Task Editor, click the Email tab.
- Select the task listing or the listing for the task step that you want to configure an email for.
- Click Add Email.
- In the Subject field, enter the subject of the email.Note:Here, as well as in the email message itself (step 6), you can type Keywords as part of your entry. For more information, see Use keywords in eSOP task text.
- In the Event Trigger field, select the option applicable to the configuration scenario.
To send the email when the... Select this option... task initiates Task Started task expires Task Expired task step initiates Task Step Started task step expires Task Step Expired - In the Message field, type the body of the email.
- In the Recipients area, perform the following procedure.
- Click Save.
- To configure additional emails, perform one of the following procedures.
- For the currently selected task, repeat steps 3-8.
- For a task other than the currently selected one, repeat steps 2-8.