Define jumps for task steps
You can configure jumps for your task if, during run time, task steps need to be skipped or repeated.
- Prerequisites
- Add task steps
About this task
Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.
Procedure
- In the Task Editor, click the AddJump tab.
- Select the listing for the task step that you want to define a jump for.
- Click the AddJump button.
- In the Name field, enter the name that you want displayed in the Task List to identify the jump step at run time.Note:
For this and any other field containing text that may be displayed in the Task List, you can type Keywords as part of your entry.
- In the Jump To field, select the target task step for the jump.Note:If you want to remove the current jump configuration, click Clear.
- Click Save.
- To configure additional jumps, perform one of the following procedures.
- For the currently selected task step, repeat steps 3-6.
- For a task step other than the currently selected one, repeat steps 2-6.