Add task steps
After you have created and saved a task, you can create the individual steps for the task. As part of this process, you can also specify other details related to the step, including expiration time, and you can override task-level personnel and equipment associations, as required.
About this task
Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.
Procedure
- In the Task Editor workspace, click Add Step.Note:If the Add Step button is inactive, either you have not established the required associations for the task and saved your input (see Create and link a task), or the maximum number of steps that can be configured based on the associated template (as noted under the pane that lists the task steps) has been reached.
- On the Details tab, in the Name field, enter the name that the system uses to identify the task step.
- In the Display Name field, enter the name that you want to be displayed in the Task List to identify the task step at run time. Do not use the same display name more than once.Note:
For this and any other field containing text that may be displayed in the Task List, you can type Keywords as part of your entry.
- Optional: In the Expiration field, use the arrow control or directly enter a value to specify the duration after which the task step should be considered expired.
- Optional: If the personnel and/or equipment associated with the task are different for the task step, select the Override Assignments check box, and then in the Assignment area, change the associations.
If you want to... Do this... change personnel resources - In the Personnel area, click Set.
The Universal Browser appears.
- Select Personnel, then select either People (for a single individual) or Classes (for a group of individuals), and then select the specific person or class.
- Click OK.
change the equipment resource - In the Personnel area, click Set.
The Universal Browser appears.
- Select Instances, navigate through the equipment model hierarchy, and then select the specific equipment resource.
- Click OK.
- In the Personnel area, click Set.
- To activate the step as part of the task, in the Status area, click the Enable button.
- Click Save.
- For each step you want to add to the task, repeat steps 1 through 7.