Activate a task
When task construction is complete, you activate the task for use in your production run time environment by enabling one or more schedules associated with the task.
About this task
Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.
Procedure
- In the Task Editor, click theSchedules tab.
- Activate the task.
If you want to activate the task in relation to... Do this... all associated schedules Click the Enable All button. individual associated schedules Select the schedule listing, and then in the Status area, click Enable. - Click Save.The task is activated.