Configure work instructions for task steps
For each step in a task, you can configure work instructions to be displayed in the Task List at run time.
- Prerequisites
- Add task steps
About this task
Note:
If the Task Editor workspace displays the grid instead of the task editing interface, select the listing for the task that you want to work on, and then click the Edit button. To return to the grid interface, click the Tasks button.
Procedure
- In the Task Editor, click the Work Instructions tab.
- Select the listing for the task step that you want to define work instructions for.
- In the work instructions workspace, enter text.Note:
For this and any other field containing text that may be displayed in the Task List, you can type Keywords as part of your entry. For more information, see Use keywords in eSOP task text. You can also insert information copied from another application, as well as graphics.
- Click Save.
- For each step that you want to define work instructions for, repeat steps 3-4.