Link a resource to a work definition

Linking a resource to a work definition helps to identify the purpose for that work definition.

Before you begin

For example, linking a material resource to a work definition helps to illustrate that the reason for the work definition is to create the material described in the associated material resource.

Procedure

  1. In the navigator, click Production.
  2. Select Work Definitions, and then select the resource you want to work with.
    Note:
    All areas that are compatible with the current resource appear. Green icons indicate a compatible view.
  3. In the Displays panel, select an editor.
    The editor appears in the workspace, displaying the resource information.
  4. Click the Details tab.
  5. In the Linked Resource area, click Change to select the linked resource from the Universal Browser.
  6. Click OK, and then click Save.