Master Segment Tab

The Master Segment tab allows you to add a master segment (that is, a work process segment set as a master) to the selected work definition.

A master segment can be associated with multiple work definitions; however, a work definition can be associated with only one master segment. Work requests are created from an individual work definition and, therefore, can also be associated with only one master segment.

When a master segment is added to a work definition, its associated details are displayed.

The following table describes the attributes specific to this resource type.

AttributeValueDescription
Add/Remove a Master SegmentUser-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 charactersDisplays the work definition segment and its associated master segment associated with the selected work definition.
Note:
Only a work definition segment with an associated master segment can be selected.
ChangeN/AClickto select the master segment to associate with the work definition.
ClearN/AClick to remove the associated master segment from the work definition.
Master Segment DetailsUser-definedDisplays the parameters and specifications associated with the selected master segment.