Work Definitions Details Tab
The Details tab offers general information about the selected work definition.
Attribute | Value | Description |
---|---|---|
Name | Required; user-defined up to 50 characters | Specifies a display name for a resource. |
Description | User-defined up to 255 characters | Provides more information about a resource that a user may find helpful. |
The following table describes the attributes specific to this resource type.
Attribute | Value | Description |
---|---|---|
Related Production Rule | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies an identification for a rule. |
Work Definition Version | User-defined alphanumeric string (A-Z, a-z, 0 - 9) up to 20 characters | Specifies the current version of this resource. |
Work Type | System-defined | Specifies the work type to describe the category of work that the work definition is associated with. Valid values are: Production, Maintenance, Quality, Inventory, Mixed, and Unspecified. |
Linked Resource | System defined | Specifies a linked resource (such as a material definition) that the work definition is associated with. Valid values are: Equipment, Material, and Personnel resources. |