Label a subprocess group

Before you begin

Note:
A resource must already have been added in order to select it from this list. For more information, see Add a resource to the workflow model.

Procedure

  1. In the navigator, click Workflow.
  2. In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
  3. In the resource type list, select a resource.
  4. In the Displays panel, click Workflow Management > Workflow Editor.
  5. Click the Workflow Editor tab.
  6. Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.
    Note:
    If required, configure the workflow.
  7. From the subprocess configuration panel, click the General tab.
  8. In the Subprocess Group field, enter a label for the group.
    Note:
    If this is a global subprocess, a default label is already entered, which you can override.
  9. Click Save.