Add a task step name to a subprocess
Before you begin
Note:
A resource must already have been added in order to select it from this list. For more information, see Add a resource to the workflow model.
Procedure
- In the navigator, click Workflow.
- In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
- In the resource type list, select a resource.
- In the Displays panel, click .
- Click the Workflow Editor tab.
- Drag and drop a Local Subprocess into the workflow and double-click it, or double-click an existing subprocess.Note:
If required, configure the workflow.
- From the subprocess configuration panel, click the Task Step Details tab.
- In the Task Step Name field, enter a name for the task.
- If required, create an expression or perform a bind to set parameter values.
- To remove the task step name, click the arrow next the property you want to clear, and then select Reset to Default.
- Click Save.