Task States
States indicate what is happening at a certain point within a running workflow.
States can be viewed in the Task History tab, a report, or in the Task Steps panel in the Task List.
States
The following tables display the different states that can be presented during run time, or through the history, or reporting:
Task States
State | Description |
---|---|
Running | in execution. |
Cancelled | Cancelled by the operator or system. |
Completed | Completed as required. |
Stopped | Stopped by the operator. |
Task Step States
State | Description |
---|---|
Waiting for Start | A manual start is required. |
Running | In execution. |
Cancelled | Cancelled by the operator or system. |
Skipped | Not executed due to a jump action or a condition branch. |
Completed | Completed as required. |
Not Started | Task step has not been reached in the execution cycle yet. |
States Displayed Visually
The states are displayed in color and graphically during run time to provide a visual clue for quick reference.
Color
The following table provides a description of the state colors:
Color | The task or task step is... |
---|---|
Green | complete |
Blue | not started |
Red | expired |
Grey | assigned to another operator |
White or Clear | currently selected |
Icons
The following table provides a description of the state icons:
Icon | The task or task step is... |
---|---|
![]() | Waiting for Start |
![]() | Running |
![]() | Cancelled |
![]() | Skipped |
![]() | Completed |
![]() | Not Started |
![]() | Stopped |