Equipment ContextShow Tasks for Equipment

You can manually set the Task List equipment context, which becomes associated with you as an operator. You must be logged in to a Task List to set the equipment context.You can manually set the Task List equipment context, which becomes associated with you as an operator. You must be logged in to a Task List to set the equipment context.

If no equipment context is linked to an operator, then the context defaults from a linked piece of equipment to the computer you are using. Otherwise, there will be no equipment context if there is no linked piece of equipment to the computer.

This feature is related to the regular Task List only, not the Web Task List or Mobile-sized Task List.

Note:
Setting the equipment context on one Task List does not affect user settings on other lists unless each list is manually refreshed.
AttributeDescription
No Equipment button OR  Use this feature to open the Set Equipment Context browser, and then select a piece of equipment. You can continue navigating to the child equipment by clicking on entries in the Equipment list.
OK Click this button to set the equipment context to the currently selected equipment.
Cancel Click this button to return to the previous screen without selecting equipment.
Clear Click this button to clear all previously selected equipment settings.

Setting the Equipment Context from the Task List

When you are in the Task List, you can add or remove an equipment context.

AttributeDescription
 Tap the equipment context icon to open the Settings dialog box, where you can toggle the equipment context on or off.
View Tasks by Equipment Context In the Settings dialog box, specify a task's associated equipment context.
AttributeDescription
Show Task for Equipment Select a piece of equipment and then slide the toggle switch on to display all tasks that are associated with a selected piece of equipment. Toggle off to hide this information.

Setting an Asset as the Equipment Context

From the Assets list, you can go to the Task List to set the selected asset as the equipment context.

IconDescription
 Tap the Tasks icon to view the tasks for the selected asset.