Set equipment context during run time

You can manually set the Task List equipment context, which becomes associated with you as an operator. You must be logged in to a Task List to set the equipment context.

Before you begin

Note:
All manual settings are overridden if a form in the Task List uses the Set Equipment Context client method to assign equipment.

Procedure

  1. To set the equipment context:
    From the...Click...
    Web Task List or Task ListNo Equipment button
    Mobile-sized Task List
    The Set Equipment Context dialog box appears.
  2. Optional: To remove previous equipment settings, click Clear.
  3. Optional: To select nothing, click Cancel.
  4. Select the equipment that you want to set by clicking through the available options, and then click OK.