The <number> represents a numeric value ranging from 0 to 5, indicating the most frequently selected reasons for a downtime.
Note: The values that appear in the L1, L2, L3, and L4 boxes for the levels of reasons are configured in the Plant Applications Administrator and are automatically populated, if available, based on the reason you select in the Top <number> Reasons menu.
Tip: Alternatively, you can select a downtime reason in the L1 box, and then select the associated reason levels, if available, in the L2, L3, and L4 boxes.