The Events page appears, displaying a list of downtime events and their details in a tabular format.
In the Events page, select and then select Add NPT to add a non-productive time (NPT) downtime event.
The Add NPT Event page appears.
In the START TIME and END TIME box, enter a duration for the NPT downtime event.
In the LOCATION section, select Click to add location. The Select location window appears. Select a department, line, and machine in the DEPARTMENT, LINE, and MACHINE sections, respectively, where you plan to add the NPT downtime event. Select Apply.
Tip: Alternatively, within the DEPARTMENT, LINE, and MACHINE boxes, in the search box displaying , you can enter the text to search for and select the required item.
In the REASONS section, select Click to add reasons. The Select Reasons window appears. Select the levels of reasons from the available reasons and then select Apply.
Note: The Click to add reasons button is enabled only when you configure the reasons for the selected machines in Plant Applications Administrator.
Optional: In the ADD COMMENT section, in the box for the comment, enter a comment for the event.
Select Save to add the NPT downtime event in the downtime events list.
Results
The newly added NPT downtime event appears in the corresponding downtime.